Cancel
Showing results for 
Search instead for 
Did you mean: 

Getting rid of next X move after a g28 U0 move

Valued Contributor
Valued Contributor

At the of the program If the move to home is radial then axial (move in X then move in Z) I output a g28 U0 to home X then output the Z move which is usually 5. If I suppress once X then  the X move would show up at with the Z move and be direct move from g28 U0.

 

I used to close the output file, let PB output X5 to nothing then reopen my output file. WIth the sync manager, I get errors re-openeing my output file. Is there a better way that people make home positioning these moves?

Using NX 8.0.3.4
2 REPLIES

Re: Getting rid of next X move after a g28 U0 move

Esteemed Contributor
Esteemed Contributor

Create a block "aluminum2_x_move", with an "X" word in it

After the g28 move, do a

 

MOM_do_template aluminum2_x_move CREATE

 

(if need be, put it in a custom command)

Then NX thinks the X has been output, and won't output it agan

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Re: Getting rid of next X move after a g28 U0 move

Valued Contributor
Valued Contributor

Thanks, that worked, can't believe I didn't know about the Create option.

Using NX 8.0.3.4

Learn online





Solution Information