Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Groove milling geometry - Limited geometry selection

Valued Contributor
Valued Contributor

Having used groove milling on a few jobs lately I have come to appreciate how nice it is, the sequencing options are a great tool to have. However I feel that it is let down by not being able to use geometry where the groove is anything other than just a linear undercut.

 

Attached are a couple of pictures where I think or hope that enhancements have been made. The first is to do with open ended grooves with lead ins or blend radii, the other is non cylindrical grooves. At present I cannot use Groove Milling as it will either ignore the radii or will refuse to machine the part at all.

 

Has Siemens looked this yet or am I the first to ask? Where do I search for existing ERs so that if submit one, I could add mine to it if there are already existing ones.

 

Regards

Adrian

 

groove-geom-01.png

groove-geom-02.PNG

4 REPLIES 4

Re: Groove milling geometry - Limited geometry selection

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The new groove operation has just been introduced.

In the past the problem was that operations had all the bells and whistles, but they didn't work properly.

In recent releases the initial release of an operation is offering the bare minimum to function and it will be enhanced as users request it or the development plan suggests.

 

You can always create an ER, the GTAC engineer will add it to an existing one, if he finds one.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX12.0.2, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX (1876) | AWC 3.4 Preparing: -

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Groove milling geometry - Limited geometry selection

Valued Contributor
Valued Contributor

Hi Stefan

Thanks for the reply, I can see how that approach would work. Start with a basic, rock solid platform before expanding, it makes sense.

Adrian

 

ER has been put in #7655734 for anyone interested

Re: Groove milling geometry - Limited geometry selection

Genius
Genius

Hello,

 

Just for referrence I have three ER for Groove Milling with one directed at the Groove milling tool they are as follows.

 

ER8274460 -- Add the ability to machine half grooves with radial groove operations

 

ER7436612 -- Add the ability to machine external radial grooves with radial groove operation

 

ER7453244 -- Please can Groove ( TCutter tools have a non_cutting definable section)

 

Just if anyone is interested in this functionality.

Regards

Dave
NX10.0.3MP13
NX11.0.1
Production
TC10
Vericut 7.3,7.4.1,8.0.2

Re: Groove milling geometry - Limited geometry selection

Valued Contributor
Valued Contributor

Those are some nice enhancements, if they get implemented it would be quite an improvement!

Learn online





Solution Information