Cancel
Showing results for 
Search instead for 
Did you mean: 

Grooving operation in turning NX9

Genius
Genius

When I try to machine groove with insert 3mm wide this is what happens:

 

machined grooves are 4mm wide,not machined are 3mm wide, multiple machined region option selected,and no rounding of corners.Why 3mm wide grooves can't be machined?

 

1.png

 

When I set 2.99 wide insert  I can machine all grooves with 2 passes each,no rounding of corners.

 

2.png

 

If I want to machine grooves with rounding of corners r0,1 , I can't machine anything.Why?

1 REPLY 1

Re: Grooving operation in turning NX9

Builder
Builder

If you assign axial trim planes or some trim points you will be able to plunge a size on size groove. However, this will only cut one groove per operation. I do not know if it is possible to do all of these grooves in one OP without either lying about the tool width or using a negative stock value in custom boundry data.

Learn online





Solution Information