Cancel
Showing results for 
Search instead for 
Did you mean: 

HOME POSITION G28

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello everyone,

Would anyone advise me how to define in CSE the function G28 U0 V0 W0?

Thanks

11 REPLIES 11

Re: HOME POSITION G28

Siemens Phenom Siemens Phenom
Siemens Phenom
Hi,

when it´s for Fanuc control, then it is already implemented (I checked NX 10 and NX1102).
It should work out of the box. Or what do you mean with "how to define"?

Thomas

Re: HOME POSITION G28

Siemens Phenom Siemens Phenom
Siemens Phenom

Please check the file Working_with_OOTB_MACH_Simulation_Examples.pdf and search for G28

in NX11.0.2 it is chapter 9.3

Here it is described where the position of G28 is defined

 

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: HOME POSITION G28

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Yes it is for FANUC. However, when I deduct G28 U0 V0 W0, nothing happens and the axes are still in the same position.

Re: HOME POSITION G28

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

So I found it and it works. Thanks

 

Re: HOME POSITION G28

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

I tried to set G28 sim simulation on sim15_millturn_9ax, but it does not work on that. I copied the home position definition to the INI file, but the axes will not move in the simulation. Need to set something up for this simulation?

Re: HOME POSITION G28

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Is the sim looking for G28 X Y Z (and you are outputting G28 U V W?)

Try outputting (use INSERT UDE if you have to) a "G28 X0 Y0 Z0", and see if that works.

If that works, but UVW doesn't, then the issue is mapping the UVW words correctly.

If XYZ doesn't work either, then it is something else.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: HOME POSITION G28

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Not even G28 X0 Y0 Z0 works. I tried it at sim13_turn_4ax and there it also does not work. I've tried everything, but none of them. At sim12_turn_2ax I have tried G28 X0Y0Z0 and G28 U0 V0 W0 and both work. I also went through CSE settings and it's the same.

Re: HOME POSITION G28

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

the OOTB G28 implementation in the Fanuc.CCF are working for single channel machine tool or I need to say for machine tools with axis names like X,Y,Z.

 

These axis names and related axis numbers are used (hard coded) inside the method GMe_GoToReferencePosition

 

To adopt it to other machine tools like sim15 with X1 Y1 Z1 etc, it is needed to copy the method into the MCF and change it. Search for hard coded axis names like e.g. "X"

 

The OOTB sim15 Fanuc will not use G28 as it is.

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: HOME POSITION G28

Valued Contributor
Valued Contributor

Hello

 

Im Having a problem with G28 as well.

Initial machine point (offset from Machine zero point) is defined in ini file.

But these values wont register. N1240P1R550 this is for X axis offset used in GMe_GoToReferencePosition.

 

But reading it in CSE simulation it show 0.

INI file is registered and it is correct file.

 

in Sim_10 G28 works and getArrayElement("AxisData", 1240, getJointNumber("X"))/GVe_dFactor shows 660 witch is correct.

So problem is narrowed down to my setup, is there any known issue that could cause this?

 

Capture.JPG

Learn online





Solution Information