Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Helical Milling in NX9.0

Creator
Creator

I am having trouble with creating a helical milling cycle to machine a non round shape in NX9. No problems with a cylindrical bore or boss.

5 REPLIES 5

Re: Helical Milling in NX9.0

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

If it is not round then your not cutting a helix. 

 

Can you post an image of what you want to cut?


@Lynn_B wrote:

I am having trouble with creating a helical milling cycle to machine a non round shape in NX9. No problems with a cylindrical bore or boss.


 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Helical Milling in NX9.0

I don't know if you mean an actual machine "cycle" - I have not seen one.

 

Round holes and bosses have hole_milling and boss_milling operations in the hole_making type.

 

To do a general helical pattern on a closed shape, I would look at surface contouring with either streamline or surface area drive method. If the drive geometry forms a closed loop, then the "Helical or Spiral" cut pattern is available.

Mark Rief
Retired Siemens

Re: Helical Milling in NX9.0

Creator
Creator

I have tried Streamline contouring with drive setting set to helical, but not having any luck.

Re: Helical Milling in NX9.0

Creator
Creator

I managed to get it to work with Streamline by setting the projection vector. Thanks for the help..

Re: Helical Milling in NX9.0

Good to see you got it going.

Another option is Zlevel with ramp between levels, and a small ramp angle. You can get a continuous path, and also G3 moves in the corners.

Mark Rief
Retired Siemens

Learn online





Solution Information