02-15-2018 10:51 AM - edited 02-15-2018 11:10 AM
Hello,
when I output one turn of helix
( exactly 360 degrees)
( XY coordinates are the same, bellow start point.)
TURN number is 1 but machine does 2 turns.
In calculation there is floor number,in this case floor of 1 is 1.
When there is more or less degrees of helix then it works.
I suppose in case of 2 turns, 720degrees, there will by TURN number 2 and machine will do 3 turns etc.
(I suppose that in mazak P number has the same behaviour on machine.)
What do you suggest for fixing this issue?
Thanks guys
02-15-2018 12:43 PM
02-15-2018 01:01 PM
02-15-2018 02:56 PM - edited 02-15-2018 03:00 PM
hi,
thank you for answer,
I was thinking about exactly the same solution but I wasnt sure if there is some any other solution or logic in helix.
sinumerik, example nc code you want to see:
G3 X-22.5 Y0. Z130. I-2.5 J0. TURN=45.