Cancel
Showing results for 
Search instead for 
Did you mean: 

Hello

Pioneer
Pioneer

How to increase the number of lines generated in the NC code? Now is up to 9999. 

2 REPLIES 2

Re: Hello

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In post builder

1) "NC Data definitions" -> Word -> Select "N"

a) Make sure the "Max" number is larger

b) Makes sure the format has enough digits

 

2) Confirm in "NC Data definitions" -> "Other Data Elements" -> "Sequence number maximum"

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Hello

Pioneer
Pioneer

Thanks, I forgot to increase digits number

Learn online





Solution Information