Cancel
Showing results for 
Search instead for 
Did you mean: 

Hidden Mapping Rules

Valued Contributor
Valued Contributor

Hello,

 

I am using NX 11 right know and I have mapped some features in NX to the MKE.

The problem is, that in the MKE my mapping rules are hidden. When i go in NX to create mapping rules

I can see the new Rules but in the MKE they are hidden.

 

 

NX 11.0.1.11
3 REPLIES 3

Re: Hidden Mapping Rules

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

If I correctly understand, you used NX command "Teach Feature Mapping" and now you want to inspect the resulting rules in the MKE.

The resulting mapping rules are stored in the configured machining knowledge xml file.

If you do not see these rules in the MKE, you must have opened an other xml file, not the one configured in NX.

Reinier Capelle
NX CAM Development - Customer Success

Re: Hidden Mapping Rules

Valued Contributor
Valued Contributor

Hi,

the thing is, that the created customization classes which belongs to the mapping rule are there even my created operations sets. Just the mapping rules are disabled. So I am pretty sure that it is the same xml file.

In NX when i teach feature mapping i can see the mapping rule which is disabled in MKE, that is how i am editing it.

Sometimes when i create the mapping rule they are saved and sometimes not...

NX 11.0.1.11

Re: Hidden Mapping Rules

Siemens Phenom Siemens Phenom
Siemens Phenom

Please send me the xml source file via pm. This sounds like something is not good.

Reinier Capelle
NX CAM Development - Customer Success

Learn online





Solution Information