cancel
Showing results for 
Search instead for 
Did you mean: 

Hole Making NX11

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Dear all

 

I am using NX11.0.1 MP1. I want to drill a hole with Hole making . But I want to select hole with diameter. how to select ? . In NX10 I am using drill type  and select diameter . 

 

Thank you 

 

 

3 REPLIES

Re: Hole Making NX11

Are you asking about specifying the hole diameter? Or about selecting holes filtering by diameter?

Mark Rief
Retired Siemens

Re: Hole Making NX11

Solution Partner Builder Solution Partner Builder
Solution Partner Builder
Dear MarkRief

I am asking for selecting holes filtering by diameter.

Thank you

Re: Hole Making NX11

Siemens Phenom Siemens Phenom
Siemens Phenom

The equivalent to the "select hole by diameter" workflow is to recognize your machining feature and use the Group Features command (either for the entire part, a subset of the features or for all features under a face).

 

This will automatically create a feature group per hole diameter. You can subsequently add operations that you need to each of the feature groups.

 

Have a look at this tech tip which was created for NX9

 

Tom van 't Erve

NX CAM Development

Learn online





Solution Information