Cancel
Showing results for 
Search instead for 
Did you mean: 

[Hole Making] Tool Drive Point

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi

 

I have a question on the Drill Depth setting.

The depth of the hole is 50mm.

I want to cutting only 40mm on the basis of Tool Tip.

I changed the Depth value to 40 with User defined.

 

hole_depth.jpg

 

However, the Depth value appears as a tool SHOULDER criterion.

 

Is there a way to solve it?

22 REPLIES

Re: [Hole Making] Tool Drive Point

Gears Phenom Gears Phenom
Gears Phenom

You can apply bottom stock.

 

Typicall the depth of a blind hole is reflected by the full diameter depth.  I have seen some drawings call out the depth as the tool tip.

 

bottom_stock.JPG

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: [Hole Making] Tool Drive Point

Siemens Phenom Siemens Phenom
Siemens Phenom

Try switching your Machining Area to MODEL_DEPTH.

hole.JPG

Re: [Hole Making] Tool Drive Point

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Thanks for the advice.

 

Machining Area is FACES_CYLINDER_1

 

When Machining Area is FACES_CYLINDER_1, Depth value is recognized as SYS_CL_SHOULDER. When Machining Area is SYS_CL_TIP, Depth value is recognized as TIP.

 

I think the depth value should be reflected in the Tool Drive Point option regardless of the list set in the Machining Area.

 

Is not it?

 

 

Re: [Hole Making] Tool Drive Point

Legend
Legend

I miss the old Point to point drilling....

Where you could specifiy the top , bottom , and move on. Now you have to deal with all this .... Its not worth the benefits ...

 


Dennis Rathi
Creations Unlimited

Re: [Hole Making] Tool Drive Point

Gears Phenom Gears Phenom
Gears Phenom

You can still use the point-to-point dialog.  You need to customize the .opt file

 

If you using NX out of the box you can edit the

 

C:\Program Files\Siemens\NX 11.0\MACH\resource\template_set\cam_general.opt file and un-comment the drill.prt

 

Restart NX and you shuld have the old Point-to-point operations.  We still use this so we can use the engage and retract options.

 

drill.JPG

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: [Hole Making] Tool Drive Point

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

First I would not alter the depth value of the feature, but use the predefined depth instead, which is much more reliable and better captures the users intent.

The NX documentation has some explanation about this subject, did you check them out?

Is the hole modeled or not?

P2P was raped in the past by users to do things it was not intended for, drilling on the other hand is focused on drilling.

If you have found an issue, report it, so that development can fix it.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: [Hole Making] Tool Drive Point

Gears Phenom Gears Phenom
Gears Phenom

I reported the Lack of the Engage motion on 1/7/2014  it was changed to an Enhancement Request and has yet to be reviewed.  Er # 7161767

 

If I could use Hole Making for everything that would be great!

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race
Highlighted

Re: [Hole Making] Tool Drive Point

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@joycejo wrote:

If I could use Hole Making for everything that would be great!


Since this is called hole making, it is focused on machining holes.

If you need multiple purpose tool paths, use generic motion. The "gmc" module is part of all modern 2.5D milling NX license packages, like NX12450, and add-ons, like NX30408 and NX30432.

P2P was only point-to-point, so it was highly raped.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: [Hole Making] Tool Drive Point

Legend
Legend

This feature recently stopped working for me, and behaves differently in NX12.0.1 than it did in previous versions. I am unable to control the SYS_CL_TIP and SYS_CL_SHOULDER. Both options give the exact same result, which moves the tool down in depth equal to the "point length". This has made a repeat job with many holes a complete nightmare for me. It will be a mess for whoever works on it next, due to all the manual depth tweaks now required. 

Glenn Balon
Production: NX 12.0.2 MP5 Primarily CAM

Learn online





Solution Information