Cancel
Showing results for 
Search instead for 
Did you mean: 

Hole Milling in NX9.0.3

Creator
Creator

We do not like the behavior of Hole Milling in NX9.  We don't use Feature based machining, yet Hole milling only uses features now.  We like the Behavior in NX8 where you can pick multiple faces and have them generate rapidly.  However, we do like having more Non-Cutting Moves like Clearance Shortest Distance.  Any chance that a future release would allow both behaviors in Hole milling (regular and feature based).

8 REPLIES

Re: Hole Milling in NX9.0.3

Hole milling does not require feature.

 

I know the UI says feature geometry, but you can just select the cylindrical faces in the holes.

 

Image2.jpg

Mark Rief
Retired Siemens

Re: Hole Milling in NX9.0.3

Creator
Creator
Mainly it is the delay in recognizing the hole and the inability to choose both a counter bore and a hole in the same operation (solid model). Also, defaults to the counter bore even though you have chosen the hole.

Re: Hole Milling in NX9.0.3

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have you tried creating a hole/boss geometry and use that?

 

I don't think they will go back to the ancient ways of doing things in CAM.

 

Using geometry groups is the preferred way anyways, so you have only one place to apply geometry changes and don't need to change 20 or more operations.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Hole Milling in NX9.0.3

Creator
Creator

That is kinda what we are doing.  We see the logic. It's just that we do quite a bit of "One Off" parts that we'll never see again.  So we are looking at up front speed rather than a long term investment in design updates/changes.

 

Thanks, Scott

Re: Hole Milling in NX9.0.3

Builder
Builder

I do not understand how it works - see image.

Select hole1 and hole2, after select hole3 see alerts. I want to milling various holes in one operation. Is it possible?

Thanks.

holemilling1.jpg

Re: Hole Milling in NX9.0.3

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What kind of operation are you using?

Can you upload the part file, so we can investigate your data?

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Hole Milling in NX9.0.3

Builder
Builder

Hole milling. Data is attached.

Re: Hole Milling in NX9.0.3

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The problem is that the holes are of different types, hole with one step and holes with two steps, see attached image.

 

To machine the two sided holes from each side separately, you must find them from each side as STEP1HOLE, which must be done manually in the machining feature navigator and not through the operation geometry dialog.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information