Cancel
Showing results for 
Search instead for 
Did you mean: 

Holemaking > Boring (no drag) > G76

Legend
Legend

G76 lets the machine bore the hole, shut the spindle off and retract away from the part wall.

The operation posts correctly except there is no dialogue for Q "shift" value anywhere

 

 


Dennis Rathi
Creations Unlimited
3 REPLIES

Re: Holemaking > Boring (no drag) > G76

Not sure, but I think Q is usually the orientation angle, and the offset is a param in the control. 

Mark Rief
Retired Siemens

Re: Holemaking > Boring (no drag) > G76

Siemens Genius Siemens Genius
Siemens Genius

Some controllers do provide more user control to define the shift amount than others. A Fanuc G76 comes with a Q to define the shift amount, the Heidenhain Cycle 202  uses a fixed value. If there is need to control this value per operation then you will need to add this parameter to the cycle definition and connect this within the post processor.

 

If so, my suggestion would be to add the "No Drag Clearance"  parameter (as already used within back countersinking\) to your cycle definition (extend by modification of your cdl):

 

SYS_CYCLE Drill_Bore_Nodrag

{

   PARAM cycle_nodrag_clearance

   {

      TYPE d

      DEFVAL "1.0"

      TOGGLE OFF

      UI_LABEL "No Drag Clearance"

   }

 

}

 

Thanks,

 

Toon

 

 

Re: Holemaking > Boring (no drag) > G76

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If I'm not adding a UDE to set all the options (e.g. Siemens with separate X, Y, Z offsets), I just use the "orientation angle" dialog value for the Q (note this is legacy PTP drill operation), as the Fanuc style G76 does not support orientation.

 

Otherwise (as stated) add a UDE or modify the cycle.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information