Cancel
Showing results for 
Search instead for 
Did you mean: 

How can I customize the point style?

Creator
Creator

The NX defaults settings for the point style is plus"+".  Can I change it to the dot"."?

If possible, could you tell me how?

 

NX version is 8.5. 

5 REPLIES 5

I'm not sure if this is a CAM issue or not. Can you tell...

I'm not sure if this is a CAM issue or not.

Can you tell us what "point style" you are asking about?

Where do you see this in the system?

Mark Rief
Retired Siemens

Re: I'm not sure if this is a CAM issue or not. Can you tell...

Creator
Creator
Hello Mark,

Thank you for your response. I'm asking about the Point of NX 3D and 2D . But, I'm sorry, I don't know how to say that exactly . When I create the point on Graphic window, I use the function below.
Menu: "Insert" / Datum/Point / Point

It creates "+" on graphic window. It is same as 2D[Sketch window],too.
I hope, You will be clear what I want to say.
I can send the image of screen shot on NX Graphic window.

Thanks and regrds,
Keiji Kimura
Highlighted

Re: I'm not sure if this is a CAM issue or not. Can you tell...

Creator
Creator
Hello Mark,

I'm sorry. I had made miss this question to your Forum.
Should I ask my question to "NX Design Forrum"?

Thanks,
Keiji Kimura

Re: I'm not sure if this is a CAM issue or not. Can you tell...

As far as I know, the plus is the NX symbol for point, and the only things you can change are the color and thickness. For sure the design forum would be the better place to ask this, or contact GTAC.
Mark Rief
Retired Siemens

Re: I'm not sure if this is a CAM issue or not. Can you tell...

Creator
Creator
Hello Mark,

Thank you for your answer.
We are migrating the CATIA V5 to NX now. We could be select the point style and we used "." with CATIA, so I asked you this question. That's my background.
Anyway, that is useful information for us. I'll ask it to the design forum, If I have a similar question again.

Thanks and regards,
Keiji Kimura

Learn online





Solution Information