Cancel
Showing results for 
Search instead for 
Did you mean: 

How can I let the B axis turning during the spindle turning and output post?

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Dear Sirs

 

Please see the video

 

(view in My Videos)

 

 

23 REPLIES

Re: How can I let the B axis turning during the spindle turning and output post?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What is machine control?

What does the control allow?

I.e. can you have blocks like: 

- "G1 X Z B"

- "G2 X Z [I K or R] B"

 

etc.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: How can I let the B axis turning during the spindle turning and output post?

Solution Partner Creator Solution Partner Creator
Solution Partner Creator
Yes!
Mazak i200 and mazatrol
I want to B-Axis turning.but I can’t show that
And I don’t know how can I do it and output post!

Re: How can I let the B axis turning during the spindle turning and output post?

Gears Phenom Gears Phenom
Gears Phenom

How to you get toolpaths like this with tool tilting?

 

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: How can I let the B axis turning during the spindle turning and output post?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I think that's new in NX12

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: How can I let the B axis turning during the spindle turning and output post?

Gears Phenom Gears Phenom
Gears Phenom

hm, can you guide me? I have NX12 and I dont now where or how to find it.

Or it is only some preview?

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: How can I let the B axis turning during the spindle turning and output post?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Sorry, I was wrong.

Tom van 't Erve gave a talk at PLMworld 2017 ("Prismatic Parts Machining Enhancements in NX 11")

 

A couple notes (from presentation)...

- preview project in 11.0.1 (round inserts) & 11.0.2 (rhombic inserts)

- Limited to tracking point P9 (center of corner radius)

 

I assume you would have to contact GTAC to get the magic ENV (or whatever) to turn this on.

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: How can I let the B axis turning during the spindle turning and output post?

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

KEN A is right.
This was the feature demonstrated at the time of version 11.0.1, with other competitors currently showing such features
However, we can not recalculate the tool path because this will cause errors.
And also can not output post by Mazak I200 or other machine 5 axis mill-turn
It is a bit puzzled.
Attach the file to provide the test.

Re: How can I let the B axis turning during the spindle turning and output post?

Valued Contributor
Valued Contributor

Attached is the PLM UGIIxxxx referenced by Ken...I think...Smiley Happy

Kal.

NX 9.0.3.4 MP12 | PB 9.0.3.2 | NX11.0.2.7 MP12 | VERICUT 7.3.4

Re: How can I let the B axis turning during the spindle turning and output post?

Gears Phenom Gears Phenom
Gears Phenom

try this. I use it to compute the holder angle.


global mom_out_angle_pos
global mom_tool_axis
global RAD2DEG

if {![array exists mom_tool_axis]} {
      set mom_out_angle_pos(0) 0.0
  } else {
      set mom_out_angle_pos(0) [expr $RAD2DEG*atan2($mom_tool_axis(0),$mom_tool_axis(2))]
}

 

But I have noticed that not every angle is computed in your case.

There is something wrong with tool axis vec.

 

example G03 X160, the tool axis  is 001, but there should be something to output your B10.

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information