Cancel
Showing results for 
Search instead for 
Did you mean: 

How do I get post builder to output drilling return to point as last Z position called before drill?

PLM World Member Pioneer PLM World Member Pioneer
PLM World Member Pioneer

Example of how I need the output to look

 

N377 G90 G0 X-.308 Y.405 S500 M3

N378 Z.5 M8M51 <------------------------- this is my return to point

N379 G82 G98 Z-.0548 R.1 F2. P700.

N380 Y3.055

N381 X8.488

N382 Y.405

N383 G80

2 REPLIES 2

Your drilling operation should have an approach move.  Th...

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Your drilling operation should have an approach move.  The Z value of the approach move will be your Z return value for the G98. 

Stan Suderman
Highlighted

the simplest approach move i have found is the Engage/Ret...

Experimenter
Experimenter

the simplest approach move i have found is the Engage/Retract in the drilling operation (you may need to put it on the default interface from the Customize dialog). It already knows the drill point and tool axis and rather than creating a point, you choose the distance. this is especially useful when drilling on cylindrical faces where the point is not on a planar face.

In the cycle parameters, for rtrcto, use 'auto'.

Learn online





Solution Information