Cancel
Showing results for 
Search instead for 
Did you mean: 

How to activate multi postprocessing?

Genius
Genius

Hi,

 

Attached Robs NXCustom variables. How can I activate a multiple cores on mi workstation, or are they active?

 

# Use Symmetric Multi-processing (SMP) if multiple processors are found
#if ${NUMBER_OF_PROCESSORS}=1
UGII_SMP_ENABLE=0
#else
UGII_SMP_ENABLE=1
#endif

 

Thanks

2 REPLIES 2

Re: How to activate multi postprocessing?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Search your syslog (Help -> NX log file) for UGII_SMP_ENABLE

if you see UGII_SMP_ENABLE = 1, you are using multiple cores for the specific functionality that is set up to use multiple cores

Note that NOT all of NX (/parasolid) code is capable of using multiple cores.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: How to activate multi postprocessing?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

From ugii_env_ug.dat it seems that it is no longer necessary to set this variable manually.

 

#  This variable enables Symmetric Multi-processing (SMP) on systems
#  with multiple CPU's or that support hyperthreading.  Performance will
#  be improved in certain Parasolid operations, such as Mass Properties,
#  Booleans and silhouette generation.  This option is only supported on
#  platforms where Parasolid supports multi-threading.
#
#     Set to 0 to disable SMP
#     Set to 1 to enable SMP
#     Unset will take the Parasolid default
#  UGII_SMP_ENABLE = 1

 

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information