Cancel
Showing results for 
Search instead for 
Did you mean: 

How to add G0 X.. Z.. in turning operations

Genius
Genius

How can I add G0 X.. Z.. After the tool change?

 If I add block G0 in initial move or after tool change, I will have

N15 T01 D01
N20 S1000 M04
N25 G00
N30 X125.334 Z14.405 M09
N35 X99.566 Z2.891
N40 G01 Z1.691 F.1
N45 Z-124.5

If I change block with G X Z

I get

N15 T01 D01
N20 S1000 M04
N25 G00 X0.0 Z0.0
N30 X125.334 Z14.405 M09
N35 X99.566 Z2.891
N40 G01 Z1.691 F.1
N45 Z-124.5


How can I get G00 X125.334 Z14.405 M09  in the same bloock?

Program & tool path>program>tool path>motion>rapid move is set to G0 X Y M09

NX 8.5

2 REPLIES

Re: How to add G0 X.. Z.. in turning operations

Phenom
Phenom

There are a few ways - one is to move that block template to initial move - where the first position is known. Others would be to use lookahead (which I don't remember if it is reliable) and another is to mark and replace the line at finish of posting. Since tool change event is so early - it can be a struggle to decide what to put there (let's say you need a move and some lines toolchange related after that move.) Sometimes it is easier to check in a later event if a tool change just happened and conditional around it (when not.)

NX10.03
Windows 7 Pro

Re: How to add G0 X.. Z.. in turning operations

Genius
Genius

Thank you!Smiley Happy

Learn online





Solution Information