cancel
Showing results for 
Search instead for 
Did you mean: 

How to add Probing Move types to Subop

Creator
Creator

Hi

The OOTB post processor probing_cycles_fanuc, has many probing types which are not found in Move type in Mill Part Probing. Is there a way to add them in Sub operations manager or any other way to use them.

2 REPLIES

Re: How to add Probing Move types to Subop

Creator
Creator

hi 

i found what i was looking for

the different probing cycles output comes based on the options selected in the existing subop

 

for example, when probing angular surface, if 3d is selected the output is with x,y cordinates and if 2d is selected the output is with Angle

 

for the bore or boss if we select specify angle then the A,B & C angles are output

 

Re: How to add Probing Move types to Subop

Glad you figured it out. Thanks for sharing the solution.

Mark Rief
Retired Siemens

Learn online





Solution Information