Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How to add a UDE into post configurator

Genius
Genius

Hello Folks

 

I am new to Post Configurator, I was wondering how to add a UDE into the post. 

I want to add a UDE to select the coolant as air(M72) or water(M73)

The following pictures show my workflow, but I can not get the output

Need help.

Thanks

 

 

$mom_sys_coolant_code($mom_coolant_type_mode)

def.JPGDEFude.JPGUDEtcl.JPGTCL editor

1 REPLY 1

Re: How to add a UDE into post configurator

Siemens Legend Siemens Legend
Siemens Legend

Hello Sean,

 

2 hints maybe solve your problem.

First one is that the mom_coolant_type_mode is the value from UDE and if you use it in your template with mom_sys_coolant_code you should set the following:

 

set ::mom_sys_coolant_code(AIR) "72"
set ::mom_sys_coolant_code(COOLANT) "73"

 

Then i just see that your template name is different to the call, remove the "set_" and it will be called. Smiley Wink

 

Following picture shows the rebuild from your information:

UDE_prob_coolant.jpg

 

And one additional hint, even if the value in the UDE options is a mix in lower/uppercase, internally it will be converted to Uppercase, it's the same for the standard mom_sys_coolant_code(xxx).

 

Best regards

Thomas

Learn online





Solution Information