Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How to add custom machine to NX CMM Inspection resource library

Creator
Creator

I want to add a new machine like "brown_sharpe" in the resource library under "D:\LocalSetup\resource\library\machine\installed_machines". I can directly place the assembly folder at this location. But in order to use it in the inspection setup, what changes do i need to make so that it is operational in the setup. should I change the database file?

1 REPLY 1

Re: How to add custom machine to NX CMM Inspection resource library

As far as I know, the CMM works the same way as CAM, so you need to modify insp_machine_database.dat.

And be sure you are working in a copy of CMM_INSPECTION\resource, not MACH\resource.

Mark Rief
Retired Siemens

Learn online





Solution Information