Cancel
Showing results for 
Search instead for 
Did you mean: 

How to create postprocessor or tcl/tk application for using three postprocessors at the same time

Creator
Creator
Czy jest możliwe aby generować 3 kody nc jednocześnie na 3 różne sterowania w tym samym czasie?
 
Posiadam 3 frezarki każda z innym sterowaniem, chciałbym linkować głowny postprocessor z dwoma pozostałymi..
 
A więc klikam sobie na obróbkę Cavity Mill generuję kod i mam trzy pliki nc na trzy różne sterowania?
 
Pozdrawiam
2 REPLIES 2

Re: How to create postprocessor or tcl/tk application for using three postprocessors at the same tim

Creator
Creator

Is it possible to generate three codes nc simultaneously on three different control at the same time?

I have 3 milling machines, each with a different control, I would like to link Main Square postprocessor with the other two ..

So I click on a Cavity operation, generating code, and I have three files nc three different control?

Regards

 
 

Re: How to create postprocessor or tcl/tk application for using three postprocessors at the same tim

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What I would do:

1) create each machine's post as a separate postprocessor (no linking)

this way you can still post to just 1 machine if you want

2) Create a separate post "Post for machine A B and C" that will do what you are asking for

 

in the "Post for machine A B and C" post

- strip virtually everything out except one PB_CMD

- that PB_CMD would use MOM_run_postprocess to run the other posts

- Note that you may want or need to close the current output file & delete it

 

Alternate:

- keep the posts separate

- use a journal to post for all the machines

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information