Cancel
Showing results for 
Search instead for 
Did you mean: 

How to define the P variables in CSE machine configurator.

Pioneer
Pioneer

Hi All,

 

I have to configure CSE drivers for the EDM machine.The controller is customised controller .

there is "parser error after reading "P10001 ="".

G92 X0.0 Y0.0
( Break In )
P10001=0.00
( BT Ignore Distance )
P10002=-0.1569
( Max Burn Depth )
P10003=-0.2914
( Break Out )
P10004=-0.100

 

How to configure the P variables in above case in machine configurator.

 

Regards

Keerti

8 REPLIES

Re: How to define the P variables in CSE machine configurator.

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

For a first time I hear that someone needs ISV for EDM. What are the reasons that you need it?

Marek Pawlus, NCmatic

Production: NX 12.0.1
Development: C#, Tcl/Tk, CSE

Re: How to define the P variables in CSE machine configurator.

Pioneer
Pioneer

So we are buiding a simulation model for mkg EDM machine.We are automating some toolpath and then checking the postprocessed out in ISV for this Machine.

Re: How to define the P variables in CSE machine configurator.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

simulating a controller NC code other than the one we do support like Fanuc, TNC, S840D etc. simple customization will not be possible. In such case the parser need to be written/customized. That is a piece of Python software, where we offer detailed documentation on NX Help, but it will be a real programming task.

 

Which controller is that, what you are looking for?

Thomas

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: How to define the P variables in CSE machine configurator.

Pioneer
Pioneer

Thanks for help Thomas.

 

The controller is the customised Fanuc controller.I can get back to you with the name,if I will get to know.

Its a MKG1000 EDM machine that all I know as of now.

Is there no workarounds available for this problem apart from customised Parser?

 

Regards

Keerti

Re: How to define the P variables in CSE machine configurator.

Siemens Phenom Siemens Phenom
Siemens Phenom

Not that I know, parser need to be adjusted to understand P parameter setting like P10001=1.

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: How to define the P variables in CSE machine configurator.

Pioneer
Pioneer

Where do I find parser file so that I can edit it .Can you please let me know how can I get the parser files ?

how can I edit it ?

 

Re: How to define the P variables in CSE machine configurator.

Siemens Phenom Siemens Phenom
Siemens Phenom

The parser of Fanuc OOTB are these ones store at the same location as MCF / CCF

CSEFanuc.py

CseFanuc_Lex.py

CseFanuc_Yacc.py

 

Please search NX Help (NX11) for "Python" in the CAM area for more details.

Please understand that we cannot fully support in programming help hereby. We will try our best to answer in the forum and give hints for help.

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: How to define the P variables in CSE machine configurator.

Pioneer
Pioneer

Thankyou for the help Thomas.

Learn online





Solution Information