Cancel
Showing results for 
Search instead for 
Did you mean: 

How to machine an area with multiple steep angles separately

Genius
Genius

area_mill_steep45_sm.pngThere is an area which has multiple steep angles

I want to machine them separately based on the steep angles range.

For example, 0-5, 5-30, 30-90 degrees, there are 3 ranges to be machined separately.

But the area milling drive method or cut regions can only set one steep angle value in the dialog.

 

Thanks

3 REPLIES 3

Re: How to machine an area with multiple steep angles separately

Siemens Phenom Siemens Phenom
Siemens Phenom
Hey Sean,

this sounds like an interesting topic for a possible enhancement.

I would like to learn more about why this would be useful for the machining process. I have an idea, but I'd be happy if you can create an Enhancement Request through GTAC, so that we can investigate your idea/ the process.

Thank you in advance!

Cheers,
Alexander
Lead Product Manager - Mold & Die

Re: How to machine an area with multiple steep angles separately

Genius
Genius
ER 9360159

Re: How to machine an area with multiple steep angles separately

Siemens Phenom Siemens Phenom
Siemens Phenom
Thx, have a great weekend
Lead Product Manager - Mold & Die

Learn online





Solution Information