Cancel
Showing results for 
Search instead for 
Did you mean: 

How to make C axis rotation in 5 AXIS machine?

Pioneer
Pioneer

Due to I want to mill slot in the part. I would like to rotated By C axis. Not move XY. Before I heard We use change a little bit angle of tool axis! But I try it..not work. Could someone show me how to fix?

Thanks!

2 REPLIES 2

Re: How to make C axis rotation in 5 AXIS machine?

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

I think you want to use the "Lock Axis" ude to lock the X or Y axis you will also need to select the plane, usually the XY plane.  This should force the rotary motion.

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: How to make C axis rotation in 5 AXIS machine?

Very interesting.

 

I tried to do the same thing. I obtain the C coordinates in the post, but they are not correctly connected with the moving origin and the ISV show a totally different toolpath.

 

Ad example if I program a zig zag pattern (floor wall), using the Ude the toolpath showed by ISV is similar to a spiral and the surface is not totally milled.

 

I think the problem is in the post, and I don't know what I need to modify.

Learn online





Solution Information