Cancel
Showing results for 
Search instead for 
Did you mean: 

How to make two surfaces one surface

Creator
Creator

I am needed to make a lot of surfaces that a curretly two only be one surface. These are not flat faces. Pictue below and NX file attached. 

Sample_A.JPG

2 REPLIES 2

Re: How to make two surfaces one surface

Legend
Legend

I can make the (2) sheet bodies one body...

 

Under surface. Use the sew option to connect them

Then under synchronous modeling I used optimize face to make them one sheet body,

It is still (2) faces, but one body

 

Is this what you are looking to do?

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Re: How to make two surfaces one surface

Creator
Creator

That worked well to make them one body thank you. Now i will have to see how well contour profile will cut them being one body.

Learn online





Solution Information