Cancel
Showing results for 
Search instead for 
Did you mean: 

How to making postprocessor for a csys rotation ?,

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Dear all

 

Hi , I want to making post for CSYS rotation .  I use  main MCS and Local CSYS Rotation (please see in attach file ).  But I want to get angle of 4th 5th of machine to milling . But mom_out_angle_pos(0) and mom_out_angle_pos(1)  is zero . How to get value of machine rotation angle in this case.

 

Thank you

3 REPLIES 3

Re: How to making postprocessor for a csys rotation ?,

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi

If you used one of generic postprocessors as initial template, you can import pb_cmd_coordinate_system_rotation.tcl Custom Command.

Or you can also reuse one of complex postprocessor templates which you can find in (...)\MACH\resource\library\machine\installed_machines\

It is working there by default.

 

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: How to making postprocessor for a csys rotation ?,

Phenom
Phenom

I am probably not remembering correctly - but look at mom_init_pos(3) and (4) and see if they represent the correct rotary position if you have an mcs main above with machine csys orientation.

NX12.02
Windows 10 Pro

Re: How to making postprocessor for a csys rotation ?,

Legend
Legend

If you use PostConfigurator you don't need to do any programming.

It is implemented by default!!

Learn online





Solution Information