Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How to output L_FREI before a tool change and at the end of a program?

Genius
Genius

How to output L_FREI before a tool change and at the end of a program? 

 

L_FREI retract to axis limit in spindle direction

L_YZM91 retract to axis limit first Y then Z

L_ZYM91 retract to axis limit first Z then Y

 

Based on the 840D Sinumerik_840D_millturn ootb template

machine DMG160FD millturn

controller: 840D SL 4.5 SP2

post builder: 11.0.2

5 REPLIES 5

Re: How to output L_FREI before a tool change and at the end of a program?

Genius
Genius
Just found out that L_FREI specially is used on DMG machine tool

Re: How to output L_FREI before a tool change and at the end of a program?

Siemens Phenom Siemens Phenom
Siemens Phenom

can you show what you want?

Re: How to output L_FREI before a tool change and at the end of a program?

Genius
Genius
I want to include the following commands before a tool change and at the end of a program;
a. L_FREI
b. L_ZYM91 (for any vertical work…ie; A-axis at 0)
c. L_YZM91 (for any horizontal work…ie; A-axis at -90)

How to set this in postbuilder

Re: How to output L_FREI before a tool change and at the end of a program?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
  1. Create three new blocks containing one word of type Text with one of the commands
  2. add the three newly created blocks to the end-of-program section in the correct order
  3. depending on your tool change location you would add it to the automatic and manual tool change sections

Post-process and see if the output is OK.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: How to output L_FREI before a tool change and at the end of a program?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You may also need to create a custom command to distinguish between the two situations with the A-axis to execute MOM_do_template with the desired M91 block. Use the custom command instead of the M91 blocks.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information