Cancel
Showing results for 
Search instead for 
Did you mean: 

How to output the total machining time in the header while post processing in NX CAM

Experimenter
Experimenter

Hi,

 

I would like to output total machining time in the NC program header while post processing it.

I heard bit about uplevel that is used in post builder to achieve it. Can anybody guide me on this or if there is any other better method to achieve the same.

I can customise the post processor to output at the end of the program but it would like to have it at the start. I am using Nx9.0.3.4 Mp05 & PB 9.0.3.1.

 

Thanks in advance.

Swamiadiyan.K

1 REPLY

Re: How to output the total machining time in the header while post processing in NX CAM

Phenom
Phenom

If you want to post process then go back and replace a marker line with time data in the header - this thread in the archive (have to be logged in) discusses it.

 

http://community.plm.automation.siemens.com/t5/NX-CAM/how-to-replace-a-line-in-a-program/m-p/254103/...

NX12.02
Windows 10 Pro

Learn online





Solution Information