Cancel
Showing results for 
Search instead for 
Did you mean: 

How to post Worpice size to NC file

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi all

 

I am try to customize post Siemens 840D for DMU 50, 

so I need create workpice size in NC file, it's like " N170 WORKPIECE(,,,"BOX",112,1,-49,-80,-100,-100,,) "

anyone can help me 

 

thanks!

Vietbay CO., LTD VN
2 REPLIES 2

Re: How to post Worpice size to NC file

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Many times a same topics was opened here..

Simple way - add UDE and define workpiece values.

More complex way - analyze each tool motion and calc minmax for XYZ and AFTER postprocessing output to first line your values for workpiece. Not so good way - for 3+2 and 5axis milling you must recalc coords - not so easy

Last way - UGOPEN application, linked with post to measure bounded part box.

The best way - insert some constant values to postprocessor (-100, 100, -100, 100, -100, 100) and edit it on real CNC...

Re: How to post Worpice size to NC file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What I use...

 

Create seed part for machine (i.e. with table, etc.)

Model box solid

User "Saves as" seed part to NC program part

adds part being machined

edits "box" solid parameters (origin/orientation/size) as needed

Post uses expressions to build WORKPIECE data

 

This works pretty well for lathes/mill-turns (where blank is always cyl/tube & along CL)

Less well for mills (part may be oriented at angle, I forget if WORKPIECE supports orienation angles, or is just square to coordinate system)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information