Cancel
Showing results for 
Search instead for 
Did you mean: 

How to post outside NX the CLSF files?

Genius
Genius

Hi all,

 

Is there any option, to postprocess outside NX CLSF files?

 

Thanks.

2 REPLIES 2

Re: How to post outside NX the CLSF files?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The old GPM was used to post CLS files.

GPM is no longer maintained and will vanish in the future.

 

In addition using UGpost, you have much more information at hand, than a CLS file contains.

 

I would suggest to not go backwards and use CLS files.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: How to post outside NX the CLSF files?

Phenom
Phenom

I agree with Stefan. The only situation where posting cl files makes sense is when other cam sytems in addition to NX are used and a common post is developed. ICAM sets up a right click postprocess launch out of NX (their customization) which creates the cl file and launches their postprocessor exe. You could also modify or add to the cl post tcl code to launch an exe when the cl file is done being written.

NX12.02
Windows 10 Pro
ITC Inc.

Learn online





Solution Information