Cancel
Showing results for 
Search instead for 
Did you mean: 

How to postprocess multiple CLSF files?

Genius
Genius

Hi,

 

Is there any way for postprocessing multiple CLSF files?

 

For Example if I have multiple program groups. Main Program and subprograms, DET_1, DET_2,_DET_3

 

My first option is to take out the whole program with all subprograms and the second option is to take out the subprograms. For example Main_Program.h, DET_1.h, DET_2.h and DET_3.h

 

Thanks in advance.

1 REPLY 1

Re: How to postprocess multiple CLSF files?

Phenom
Phenom

If you are asking about making separate cl files when posting a parent group - the cl post could be modified to do that - or the postprocessor could key on a message in the group to do it. Neither are OTB in NX to my knowledge.

NX12.02
Windows 10 Pro
ITC Inc.

Learn online





Solution Information