Cancel
Showing results for 
Search instead for 
Did you mean: 

How to program a tool that mounts on a manually indexable head?

Creator
Creator

Hi.

 

I need to program a square shoulder mill which mounts on a manually indexable head and the control point (tracking point) should be at the lowest point of teh cutter after it is indexed.

This is a roughing operation and has to work with a 'workpiece' geometry.

 

Thanks in advance!

 

-

Girish

5 REPLIES

Is this like a right angle head but you can rotate the to...

Gears Phenom Gears Phenom
Gears Phenom

Is this like a right angle head but you can rotate the tool as needed?

 

If so you will need to add a Head object and then have the tool as a child of the head.

 

You will need to set the unit vectors for the direction from the spindle axis.

 

head.JPG

John Joyce, Manufacturing Engineer,
Senior Aerospace
Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Is this like a right angle head but you can rotate the to...

Creator
Creator

Hi camster. Thanks for your reply.

I did try to define a head and a child tool. The tool path generated by this tool was no different as opposed to the tool path produced by the same tool without the head.

I need NX to recognize the effective cutting shape of the tool in that orientation and calculate the tool path.
HEAD.JPG
-
GN

Hello Camster,   I have this configuration. But I don't k...

Genius
Genius

Hello Camster,

 

I have this configuration.

But I don't know, how can I load the 3D head object on this tree. With proper configuration I could see the head, holder and the cutting tool, all 3D models on NX CAM.

tool_tree.jpg

Re: Is this like a right angle head but you can rotate the to...

Gears Phenom Gears Phenom
Gears Phenom
When you create the tool path does the tool axis match the vector? Is this s fixed axis operation of variable axis?
John Joyce, Manufacturing Engineer,
Senior Aerospace
Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Is this like a right angle head but you can rotate the to...

Creator
Creator
You are right, this is a fixed axis operation of a cutter on a pre-fixed tilted and rotated tool axis. When I create the tool path the tool axis was set to 'Z' axis. I did manage to get the tool path by using an alternate method - but I need to know how to do this in an automated operation in NX.
Thanks for helping.

-
GN

Learn online





Solution Information