Cancel
Showing results for 
Search instead for 
Did you mean: 

How to set up simulation for tool magazine

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi

I made a five - axis machine tool magazine, how to make its rotation.

Should I modify the Machine Configurator file? The Machine Configurator file has been set the password, how can I do the modification?

1.jpg2.jpg3.jpg

1 REPLY 1

Re: How to set up simulation for tool magazine

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

there is a sample machine (SIM11) available in the OOTB samples from NX CAM Simulation which shows the movement of a turret. You can reuse this for your project.

 

Lool at the ToolChange.prg file which is located under ...mach\resource\library\machine\installed_machines\sim11_turn_2ax\cse_driver\fanuc\subprog\ToolChange.prg

 

Within the subprog there is MOVE command written in AC language (not in NC language) to move the component to a desired position. In your case this is more flexible because you don´t have to do modification within the Machine Configurator. You can write the program with the text editor of your choise. You only have to ensure that the NC command e.g. M6 calls this subprogram. 

 

The parse error comes up due to the uncommented ##LANGUAGE NATIVE line 82 --> this is independent of your request.

 

I suggest that you go first stepwise through the sim11 sample to understand the workflow and technic

...\mach\samples\nc_simulation_samples\sim11_turn_2ax_cam_fanuc_mm.prt

 

Thomas

Learn online





Solution Information