Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: How to slowdown tool before entering an arc

Creator
Creator

Ok, so I created a completely new part and i am now experimenting with the optimize feed rate parameters. what I found out is that if I use nominal stepover less than 2mm, and the feed rate is set to 420, the engage movement will be 420, but then the whole feedrate is slower than 420 and even slower in the corner with cylinder, if i use nominal stepover greater than 2, the whole feed rate will be 420 but the slowdown wont be near close to 80 as i want it.

 

the closest i got is the 1st picture where it goes 89 in arc, but to be honest, my knowledge about NX is very limited, actually I learned a large deal just by trying out the stuff you suggested, and this method with adding extra blanks and then trying to maybe hit the feedrate you know you need, seems to me pretty time consuming.

 

Why I am actually trying to have a variable feedrate is becaouse as i said i work with wood and along the grain you can machine alot faster than perpendicular to grain, so i wish to save as much time as possible since i'm producing more than few of this product, and since the material is soft it tears out pretty easily in some areas, and those are the areas that i want slower feedrate, the feedrates i want are tested.

 

 

Re: How to slowdown tool before entering an arc

Creator
Creator

Its funny how simple things can be so frustrating, I selected part and blank in workpiece and now it does slowdown

Re: How to slowdown tool before entering an arc

Creator
Creator

Hi SvenV, I tried dividing face as you said, but I cant seem to be able to divide the toolpath, maybe i used wrong command?

Re: How to slowdown tool before entering an arc

Valued Contributor
Valued Contributor

Select the top face as part boundary and click ok.

Go back to Part Boundaries --> Edit.

Here you can cycle through the selected curves using the arrows and give each an custom feed rate. (The selected curve is highlighted in orange)

 

Attached you can find a picture and the file.

 

Regards,
Sven


Regards,
Sven

NX11.0.1

Re: How to slowdown tool before entering an arc

Just confirming the blank has to be in the workpiece for Optimize Feedrate. It uses the IPW, which requires a blank in the geometry parent, not the operation.

The other approach here seems to be custom feedrates, which can be on boundaries or faces. This may work, but it will be very tedious if you want gradual slowdowns. That's why I tried the triangular blank on the corner - so the system woudl adjust the feedrate gradualy. 

Mark Rief
Retired Siemens

Re: How to slowdown tool before entering an arc

Pioneer
Pioneer

how can I see the feed rate values on the 3D model in operation navigator mode

Re: How to slowdown tool before entering an arc

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you mean how to display the feedrates in the graphics window as you generate/replay a tool path...

Edit the operation -> Display options -> In the "Path" block expand the "More" sub-block -> "check" the option "Feed Rates"

 

This is also available in (method view) "Method" objects (which I assume is inherited by the operations in the method)

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: How to slowdown tool before entering an arc

Pioneer
Pioneer

worked. thanks.

Learn online





Solution Information