Cancel
Showing results for 
Search instead for 
Did you mean: 

How to use synchronization

Creator
Creator

Hello,

i just want to know use of synchonization in NX-11 CAM

please help me.

9 REPLIES 9

Re: How to use synchronization

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

As in synchronizing multiple channels (turrets) on the machine tool?

if so, see here:  https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_help/#uid:xid1128418:index_mfgadv

 

Or something else?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: How to use synchronization

Creator
Creator

Actualy we want to know the license which is used for synchronization for mill turn (dual turrets),

we are using TOTALMACH (license) but not responding for synchronization, please help me in this.

 

Re: How to use synchronization

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

You need the NC Simulation Add-on (NX30434) in order to run the sync manager.

 

~U

 

 

Re: How to use synchronization

Siemens Phenom Siemens Phenom
Siemens Phenom

According to the price book you should have the sync manager, if in fact you do have total machine NX13430. Simulation is not a requirement for sync manager since NX4, but it will make programming easier.

 

ScreenHunter_02 Jun. 15 13.19.gif

Re: How to use synchronization

Siemens Phenom Siemens Phenom
Siemens Phenom

Try opening up this file, Select PROGRAM, RMB, Toolapth -> Synchronize. If it works  you have a license.

 

MACH\samples\nc_simulation_samples\sim13_turn_4ax_fanuc_cam_mm.prt

Re: How to use synchronization

Creator
Creator

I opened that file, but i am unable to post that file. please help me.

Re: How to use synchronization

Siemens Phenom Siemens Phenom
Siemens Phenom

Start NX, from Gateway, File Utilities, Select Bundles, make sure you are using TOTALMACH

 

 

ScreenHunter_05 Jun. 15 14.13.gif

Re: How to use synchronization

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi Eranna, as people already mention you need to have a Synchronisation Manager license. This license is not availible as seperate add on. It is included inside Total Machining it also is included inside NX30434 Simulation add on.

 
Highlighted

Re: How to use synchronization

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Please also note you can not just Post a Synchronized Programm out of NX CAM. Postprocessing can only be done by Synch Manager. For this you need the license. If you say you  can not post, does this mean you see synch Manaer or you get an error and synch manager is not opening? In this case it maybe is a license issue!

Learn online





Solution Information