Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How use facets as a blank for cavity milling?

Pioneer
Pioneer

Hi colleagues,

I remember the possibility to use facets as a blank in previous versions of NX. I could create a facet from simulation and added it as a blank for the next operation. Now when I select a facet as a blank in cavity operation, it doesn't take it... Do you have any ideas?

3 REPLIES 3

Re: How use facets as a blank for cavity milling?

Gears Phenom Gears Phenom
Gears Phenom

hi,

as I have tested it in NX 12.0.2.9 mp04 it is working

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: How use facets as a blank for cavity milling?

Legend
Legend

like @Juraj said,that issue was fixed  NX12.0.2 MP2

 

now MP5 is available,you can download and install.

-----------------------------------------
NX 12.0.2.9 MP10 / Testing NX 1847 Version 1867
CanikSoft NC Post-Processing & G-Code Simulation
www.plast-met.com.tr
www.caniksoft.com

Re: How use facets as a blank for cavity milling?

Pioneer
Pioneer

Thank you! I've started the downloading process. Thank you!

Learn online





Solution Information