Cancel
Showing results for 
Search instead for 
Did you mean: 

I have Questions About Contour Area..

Pioneer
Pioneer

MS2.jpgMS1.jpg

I want to make the Path like above picture.

 

But I do not know how to make a Contour_area of NX CAM.

 

What should I do?

 

 

I've attached a file.nx1.jpg

10 REPLIES

Re: I have Questions About Contour Area..

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

One way is to WAV link the part, delete the angle face with Synchronous Modeling and then pick those faces to machine.  

Jeff Sauers, Lead CNC Programmer, Oberg Industries

Production: NX 10.0.3.5, Vericut 8.0


Re: I have Questions About Contour Area..

Valued Contributor
Valued Contributor

From what I gather your problem is that it is not cutting the air? From my days in mastercam we would extract surfaces from the body, extend surfaces and then trim. NX should be able to do the same thing. Hopefully somebody can give a better solution where you don't need to modify geometry.

Using NX 8.0.3.4

Re: I have Questions About Contour Area..

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

With "roll over edges" turned off in the cutting parameters, NX will strip the path that moves over the edge.

 

You can turn this on and use a trim boundary to get the path you expect.

Without the trim boundary, NX might not keep tangent to the edges of the milling area.

You can try first without the trim boundary to see if it is really needed.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: I have Questions About Contour Area..

Genius
Genius

See atatcehd file created in NX 7.5. Used default settings.

 

Hope this helps

 

BR,

Mak

Re: I have Questions About Contour Area..

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Here is the same prt file in NX 9.0.3 used boundary as drive method.

 

Hope this helps

Frank Bartucci
NX CAM COE

Re: I have Questions About Contour Area..

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor
if you can wait for NX 10.0.2 there will be a option under "Cutting Parameters" --> "Strategy" --> "Extend Path" check the radio button "Extend Across Undercuts"
Frank Bartucci
NX CAM COE

Re: I have Questions About Contour Area..

@FDB is right. This was added to allow you to revert the the old behavior of cutting air if needed.

Mark Rief
Retired Siemens

Re: I have Questions About Contour Area..

Pioneer
Pioneer

Mark,

 

Is there a "whats new" pdf document of 10.0.2 availible right now?

 

Regards,

mlewan

 

Re: I have Questions About Contour Area..

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The release is planned for end of July, if everything runs well, so you will have to wait for that release date.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information