Cancel
Showing results for 
Search instead for 
Did you mean: 

I have a problem want to everyone help to me!!

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Dear all

 

I have a POST problem need help

 

when i have a 3+2 axis machine ,type is   table - head

 

S__35405840.jpg

 

 

Like it

 

my control is fanuc

 

when I want to go  " B "  =  90°   .  I want go to " X 、Y  "  first   ,second go to " Z"

 

But when I want to go " B " = 0~89° . I want go to " Z "  first , second go to "X,Y"

 

Hope you can give me some help ?

 

Thanks!   Very thanks !

6 REPLIES

Re: I have a problem want to everyone help to me!!

Juraj 1st Gear
1st Gear

why do you want to go first Z when operation is at some B angle?

Show part of your nc code.

 

Simple answer is output Z first / then post will output XY and omit modal Z.

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: I have a problem want to everyone help to me!!

Ken_A 1st Gear
1st Gear

Would this be "initial / first move" only, or all rapid moves?

Does the machine have any coordinate system rotation options (G68 or ?)?

 

What I would do to accomplish your logic is to add a custom command to the rapid move event.

Add a call to the custom command BEFORE the "G0 X Y ..." blocks in the "Rapid" move event.

Test on mom_out_angle_pos(0) or mom_out_angle_pos(1)  (respectively, the 4th & 5th axes as defined in your post).

 

Note you may need more logic, e.g. for a vertical 3 axis mill,

- if you are going DOWN in "Z", typically you want to move "XY" then "Z"

- if you are going UP in "Z", typically you want to move "Z" then "XY"

 

You could add a block "cadex4_move_z" with "G0" and "Z" words

-if you want "Z" first, "MOM_do_template cadex4_move_z"

-else use a "MOM_suppress once Z", then after the normal output, add a call to "MOM_do_template cadex4_move_z"

 

You may want to turn off "work plane change" option in the rapid move event as well.

 

Another option might be to over-ride "MOM_rapid_move" proc in the post and write your own logic (IIRC, that already has some testing for tool vs. machine axis)

 

But (as with the other poster) I would suggest you think through what you are asking.

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Re: I have a problem want to everyone help to me!!

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Sorry! I made a mistake  ~

 

Tilting surface B-1 ~ B-89 degrees, the first move to go X, Y, After go Z.

 1.jpg

 

Lateral plane simply B-90 degrees, the first move to go Z, After go X, Y.

 

2.jpg

 

I send my POST  at attached file .

 

Can you give me a answer.   Thanks!

Re: I have a problem want to everyone help to me!!

Juraj 1st Gear
1st Gear

Just tell me why do you want first Z in second case.

Because if the spindle is on the left, so there is no need to output first Z and then XY.

 

Anyway if you want to do that just execute one Z move before XY.

Check attachment.

-------------------

Best solution is sequence:

-M128 (manually added)

-XY (manually added)

-Z (manually added)

-M129 (manually added)

-Plane function /cycle 19

-XY (this move do nothing, you are already there)

-Z (this move do nothing, you are already there)

 

--> and your first move will be always horizontal and then vertical

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: I have a problem want to everyone help to me!!

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Dear sir

Because the actual position of my spindle above the workpiece.
when the spindle rotation 90 , the first move XY is dangerous

 

And Thank you very much for your answer

This is my answer.

But I don't know how did you show it?

I only see a  Discriminant

Can you tell me how to do it??

 

Also I will test the best solution you give. 

But I do not know whether their machine can support "M128"

2017-08-07_00-58-44.png

Re: I have a problem want to everyone help to me!!

Juraj 1st Gear
1st Gear

Because the actual position of my spindle above the workpiece.
when the spindle rotation 90 , the first move XY is dangerous

- when you move spindle on the left (x minus - maybe X0 M91 ) you have maximum space to position XY and then Z.

If angle is -89 - do you have enough space for XY and then Z? probably not.

I always position spindle on the left where it can be safely rotated and it is good position to reach first point of the path safely.

But I mentioned "best " solution - this could works. And you have not to move spindle on th left.

It will reach the position safely.

(*I forgot, Remember when you are using M128/tcpm reset mom_pos by mom_mcs_goto)

 

But I don't know how did you show it?

I only see a  Discriminant

Can you tell me how to do it??

I dont undestand what you want now.

You found  PB_CMD_your_z - ok

Template "your_z" is in the nc block tab where is every block stored.

This custom command PB_CMD_your_z is called in custom command PB_CMD_define_work_plane.

that is all.

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information