Cancel
Showing results for 
Search instead for 
Did you mean: 

I have a question about Planer mill.

Pioneer
Pioneer

 

 1.jpg

 

 I am going to cut red section with Ø12 Flat .

 

 First. I used Z-level Profile.

 

 zlevel.jpg

 

  I like Z-level. because it is no jump and no plunge.

 

 In other words.

 

 one engage, one retract. and using Stagger ramp on part.

 

 But, Planar_mill have to many jump and plunge.

 

 planar_1.jpg

 to many jump...

 

 

 planer_2.jpg

and plunge..

 

I want to use the Planar mill as Z-level

 

What should I do?

 

planar_3.jpg

 

 

 please help and thanks.

5 REPLIES 5

Re: I have a question about Planer mill.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

Is there a reason why you are not using the Hole Milling operation. It gives you the ability to use a Helical Cut Pattern which most customers seem to prefer?

 

Hole_milling.jpg

Tom van 't Erve

NX CAM Development

Re: I have a question about Planer mill.

Pioneer
Pioneer

yes I know hole milling.

 

but sometimes hole milling can not selected iges modeling.

 

thank you for your advise.

Re: I have a question about Planer mill.

Siemens Phenom Siemens Phenom
Siemens Phenom

As a bare minimum, you can even use hole milling on just a point where you manually define the direction, depth and diameter of the feature to machine. Wouldn't that be easier?

 

I will be happy to try and help if you can share a sample IGES model that is causing difficulties.

 

Tom van 't Erve

NX CAM Development

Re: I have a question about Planer mill.

Legend
Legend

If you want to use 2d use Finish Wall.

 

Set your boundary at top of part, set your floor, and put cut level bottom only. Change your engage open to same as  closed and then set  closed as ramp on part at whatever  angle  you want.

 


Dennis Rathi
Creations Unlimited

Re: I have a question about Planer mill.

Phenom
Phenom

Before hole milling we used to calculate the helical diameter as a tool % 

 

100*(HoleD-ToolD)/ToolD

 

Use helical engage and floor only

Need separate operations for different diameters

This was to get Helical output instead of linear that ramp on shape output.

 

Homemaking should get you there

If the iges is a solid try "Heal Geometry" & "Optimise Face" it will often help

Or manual define holes on points

Learn online





Solution Information