Cancel
Showing results for 
Search instead for 
Did you mean: 

I'm looking for the solution of this alarm.

Experimenter
Experimenter

Hi guys, good day! I need your sugestion, recommendation and sulotion about my problem. This is my first time that i used haas vf2 5x. (3+2) machine.I'm trying to input  my nc data into haas vf2 5x (3+2) machine, but i found some alarm. The alarm is ( 430 unexpected end of input).

Please see the screen shot sample nc data program here.

Thank you very much.

 

Capture.PNG

21 REPLIES 21

Re: I'm looking for the solution of this alarm.

Experimenter
Experimenter

The screen shot NC data is come from NX 11. 

Re: I'm looking for the solution of this alarm.

Siemens Phenom Siemens Phenom
Siemens Phenom

Should the first line be %O00031 ? with upper case O?

you have

%

o00031(lower case o)

Re: I'm looking for the solution of this alarm.

Legend
Legend

Your Z values seem crazy big...

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Re: I'm looking for the solution of this alarm.

Siemens Phenom Siemens Phenom
Siemens Phenom

I believe it does not like the : in the time stamp, or any where else, change it to a -

Re: I'm looking for the solution of this alarm.

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

I have seen on some Haas machines where the End Of Block character is needed at the end of each line.   I think it is a Semicolon ;

 

You can add this from Post Builder N/CData Definitions - Other Data Elements End of Block

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: I'm looking for the solution of this alarm.

Did you get the alarm immediately or was some of the program inputted into the control?

 

Do you have a % at the end of your program?

 

Also, from other Haas programs I have seen which were proven Haas VF milling programs...

% by itself should work.

O000031 should be fine but there may be a character limit.

An O-name is optional so you can leave it out.  I see this frequently.

Colons are acceptable characters.

There is a character limit to comment lines but I'm not sure what it is, I cannot find my notes on it and Haas manuals are infamous for incomplete information.

NX 12.0.2

Re: I'm looking for the solution of this alarm.

Siemens Phenom Siemens Phenom
Siemens Phenom
Does it error while loading? If not run it in single block until it errors.

Sent from my Android phone using TouchDown (www.symantec.com)

Re: I'm looking for the solution of this alarm.

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi Mould united, thank you for your responsed. I got the alarm during i tried to load my nc data into haas machine. yes i have a % sign in my end of program. what do you mean in (An O-name is optional so you can leave it out) eg, O000031 it becomes 000031? i have attached here my nc data.. please see. thank you for your responsed. 

Re: I'm looking for the solution of this alarm.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Chrisss

Do you have a program on the machine that you can download to your PC and look at the of the header and end of program?

Regards

Paul

Learn online





Solution Information