Cancel
Showing results for 
Search instead for 
Did you mean: 

I'm looking for the solution on this alarm. (817 INCORRECT ARC DATA)

Creator
Creator

Hello all,

Good Day, I had encountered cnc alarm, which is (817 incorect arc data. it is post Post processor error right? how can i edit my post processor using post builder to solve this error? 

 

please see the image.

 

thank you for the sugestion

31206370_1968947673178975_635368633949749248_n.jpg

6 REPLIES

Re: I'm looking for the solution on this alarm. (817 INCORRECT ARC DATA)

Gears Phenom Gears Phenom
Gears Phenom

I don't see any I or J in the next G2 move  - you may need to force them in the post.  Some controls require this even if it is the same as the previous

 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: I'm looking for the solution on this alarm. (817 INCORRECT ARC DATA)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Usually I and J are set to modal, you just need to remove the modality.

This is preferred over forcing the output.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: I'm looking for the solution on this alarm. (817 INCORRECT ARC DATA)

Solution Partner Creator Solution Partner Creator
Solution Partner Creator
Hi Stefan Pendl,

Good Day! where i find and set modal? it is inside in the post builder or inside of my program parameters.?
thanks.

Re: I'm looking for the solution on this alarm. (817 INCORRECT ARC DATA)

Solution Partner Creator Solution Partner Creator
Solution Partner Creator
Hi John Joyce, good day, yes correct. G2 need I and J but the problems is, in my NC data i saw dont have any I and J while the other g2 blocks have. i dont know if it is because of my post procesor. thanks.

Re: I'm looking for the solution on this alarm. (817 INCORRECT ARC DATA)

Creator
Creator
Hi John Joyce, thank you for your support. already solve this issue.

Re: I'm looking for the solution on this alarm. (817 INCORRECT ARC DATA)

Creator
Creator
Hi Stefan PendI, good day. thank you for your support. already solve this issue.

Learn online





Solution Information