Cancel
Showing results for 
Search instead for 
Did you mean: 

I wants the milling taper teeth,How can I do?

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Dear all

 

Can we do the taper spiral?

The customer wants the milling taper teeth .. but is the customized taper angle

If you want to do milling, what good way?

 

2017-08-07_01-50-16.png

4 REPLIES

Re: I wants the milling taper teeth,How can I do?

Siemens Legend Siemens Legend
Siemens Legend

I guess you would like to have a toolpath that looks like a helical motion. Today, you can do that with a Z-Level-Profile operation by setting the Level to Level with Ramp on Part and setting the Ramp Angle you want (See the attached picture).

 

We are looking forward to introduce a new Helical option as a Steep Cut Pattern in future versions.  

 

I hope that is what you needed. If not, please feel free to clarify.

Re: I wants the milling taper teeth,How can I do?

I think you are asking about a tool path for machining tapered threads? When you say "teeth" are you talking about cutting a tapered pipe thread?

 

I am using NX10.0, and only see regular "helical" thread mill options. I'm not sure if there is a "tapered thread mill" option in NX. Hopefully a guru will jump in and let us know if that is possible somehow. (For comparison, Mastercam has supported cutting tapered threads for at least a decade...)

Re: I wants the milling taper teeth,How can I do?

Stefan_Pendl 3rd Gear
3rd Gear

NX will automatically create a tapered thread tool path for NPT threads, as an example.

You only have to use the thread milling operation.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk Testing: NX12.0 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink

How to Get the Most from Your Signature in the Community

Re: I wants the milling taper teeth,How can I do?

Ken_A 1st Gear
1st Gear

If you need a different taper angle, however, (IIRC) NX threadmilling doesn't allow editing of the taper angle.

You can define a tapered helix curve, then use (I thonk) FASC & drive method = "curve"

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
Apparently I've turned into a gearhead


Learn online





Solution Information