Cancel
Showing results for 
Search instead for 
Did you mean: 

I would like to set the decimal point.

Pioneer
Pioneer

Hi. Engineers.

 

As I understand it, I know the default setting to point 16 digits.

 

But I want to use only three decimal places. What should I do?

 

 

Cut_Level_Decimal.jpg

2 REPLIES 2

Re: I would like to set the decimal point.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You can't change the display in the dialogs as far as I know.

The system will always consider double precision.

 

The post-processor will output to what ever precision you tell him to.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: I would like to set the decimal point.

The system stores double precision - you cannot change that. Like @Stefan_Pendl said, it is the job of the post to round off to the correct precision for the control.

 

The display in the dialog is an NX-wide setting:

 

Menu > Preferences > User Interface > Options > Dialog Boxes > Decimal Places.

 

Also found in Customer Defaults > Gateway > ...

Mark Rief
Retired Siemens

Learn online





Solution Information