Cancel
Showing results for 
Search instead for 
Did you mean: 

IPW / CUTTING_SPUN

Valued Contributor
Valued Contributor

Hello!

I've a question to working with CUTTING_SPUN in tool. My tool looks like this:

2016-02-03 09_25_04-NX 10 - Wkz-Maschinen-Designer  - [63000077.prt (Schreibgeschützt) ].png

The red part is the CUTTING_SPUN.

First I have an operation for pre-drilling, but the pre-drilling-tool actually is to small for the tool that follows (the tool you see above). You see it in the toolpath-visualisation:

2016-02-03 08_52_24-I__NX10_windows64_MACH_resource_library_tool_graphics - Clover.png

Also in simulation the system detects an collision between tool and IPW:

2016-02-03 08_53_45-NX 10 - Fertigung - [D1758478_0.prt (Geändert) ].png

Till here everything is OK. But if I want to see the IPW after this operation the IPW looks like this:

2016-02-03 08_53_01-NX 10 - Fertigung - [D1758478_0.prt (Geändert) ].png

I think it should look like this:

2016-02-03 08_54_15-NX 10 - Fertigung - [D1758478_0.prt (Geändert) ].png

What's your opinion?

 

Werner

Werner
Production: NX12.0.2, FBM | TcUA 11.4.0.6
Development: VB.NET, Tcl/Tk
3 REPLIES 3

Re: IPW / CUTTING_SPUN

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Werner,

 

do you see the "wrong" result in Verify AND simulation?

What about "Machine Code based" in simulation.

 

Make sure you have set inside the "simulation Settings" "In Process Workpiece" group the "Tool Shae" to --> Assembly.

 

In which version do you see that behaviour?

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: IPW / CUTTING_SPUN

Valued Contributor
Valued Contributor

Hi!

I work with NX10.0.3.5

Please look at the attached video.

(view in My Videos)

 

Werner

Werner
Production: NX12.0.2, FBM | TcUA 11.4.0.6
Development: VB.NET, Tcl/Tk

Re: IPW / CUTTING_SPUN

Siemens Phenom Siemens Phenom
Siemens Phenom

Ok I see it is about "Show 3D IPW". That feature takes the IPW stored inside the operation. Make sure the stored IPW includes the correct one by run Visualize (Verify) 3D and Assembly and activate "Save". If afterwards Show 3D IPW still shows the wrong IPw please contact GTAC.

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information