Cancel
Showing results for 
Search instead for 
Did you mean: 

IPW autoupdate

Pioneer
Pioneer

Hello,

 

is there a way to let autoupdate the IPW ?

Example: 1 Manufaturing Part 2 Workpieces - in the secounf is the IPW. After i change something in the first, i need to keep in mind to update the IPW in the secound.

Is there something like that ?

NC Programmer
NX 11.0.1.11
3 REPLIES 3

Re: IPW autoupdate

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

At the moment it is not automatically updating it. We might enhance this in the future but so far there are no concrete plans.

 

Thanks,

Oliver

Re: IPW autoupdate

Legend
Legend

Autoupdate seems like the go to method!

 


Dennis Rathi
Creations Unlimited

Re: IPW autoupdate

Experimenter
Experimenter

Yes, create one workpiece that only has the blank selected. Then inside place your two additional workpieces that only contain the part. Or only place multiple MCS inside the Blank, then pick geometry in the operations.

 

blank_geo.JPGblank_selected.JPG

Learn online





Solution Information