Cancel
Showing results for 
Search instead for 
Did you mean: 

IPW module error

Genius
Genius

Hello Folks,

 

I have a program group including two floor wall millings, the first operation is cut by a solid tool assembly, the second operation is cut by a parametric model.

 

When I do the Tool Path Verification, I have an IPW module error:

Capture.JPG

 

Thanks

3 REPLIES 3

Re: IPW module error

Siemens Phenom Siemens Phenom
Siemens Phenom

And what does the logfile tells you?

In which NX verison you are?

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: IPW module error

Genius
Genius

Hello Thomas,

 

I am using NX 11.0.2

 

>>>> Error code 3295018 caught in file "D:\workdir\Patches\nx1102_patch\src\camsutilint\no\ind\ui_verify.c" at line number 9365
Read in partition for part "T:\xxx.prt", cpu 0.016, real 0.003
Partition info: PATH:1 (0.0, 0.0)
Loaded 1 partitions from T:xxx.prt cpu 0.016, real 0.003
Read in partition for part "T:\xxx.prt", cpu 0.000, real 0.003
Partition info: PATH:1 (0.0, 0.0)
Loaded 1 partitions from T:\xxx.prt cpu 0.000, real 0.003
TP Exception: Exception from boost::geometry: Dynamic exception type: class boost::geometry:Smiley Surprisedverlay_invalid_input_exception
std::exception::what: Boost.Geometry Overlay invalid input exception

*** EXCEPTION: Error code 3295018 in line 2211 of D:\workdir\reference\NX1102_7\src\dctkloader\no\ind\dctk.c at Thu Apr 11 11:51:10 2019 Eastern Daylight Time
+++ Error in IPW module. See syslog for details.

Re: IPW module error

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello SeanHAI,

 

this looks like a problem in the software and we have fixed some in that area in the past. I suggest to use a newer version of NX and in the case this problem still exists then I like to ask you to open a IR through GTAC.

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information