Cancel
Showing results for 
Search instead for 
Did you mean: 

IPW turn first, mill and then finish turn

Master
Master

I am turning a part and then doing some milling and then finish turning the part and the IPW is reverting to uncut when I get back to the finish turn operations. I had the milling at the end but wanted to mill at high chucking pressure so I needed to put it before the finish ops. Any ideas why? Using integrated NX 11.0.2.7 mp12.

 

 

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000
13 REPLIES 13

Re: IPW turn first, mill and then finish turn

Phenom
Phenom
This has worked for me. I switched back and forth a few times.
NX12.02
Windows 10 Pro
ITC Inc.

Re: IPW turn first, mill and then finish turn

Master
Master

Thank you! 

I just tried that tree setup and it still showed the IPW reverting. I am using a generic motion operation and am wondering if that is what is causing the issue.

 

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000

Re: IPW turn first, mill and then finish turn

Phenom
Phenom
Maybe the spindle (turning mcs) being parent and then having turning workpiece and mill mcs at same level is important. Didn't yours have mill mcs parents and mill mcs not on same level as turn workpiece? It is finicky. Plus you have to keep generating ops above sometimes.
NX12.02
Windows 10 Pro
ITC Inc.

Re: IPW turn first, mill and then finish turn

Master
Master

I put it in this order which looks pretty much identical to yours and it still does the same thing. The one pic shows the stock being there when It should only have .25mm stock.

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000

Re: IPW turn first, mill and then finish turn

Valued Contributor
Valued Contributor

Brad.
It's a known issue with NX MillTurn setup. Template subtypes (Mill Control, Lathe Control & Generic Motion) cause havoc on the setup.
My workaround is to make(cheat) a separate millturn setup for these subtypes...limitations is when using them for machining...which I've been avoiding...
Finally below is the NX setup I use.

 

 

NX MillTurn Setup.png

 

Kal.

NX 9.0.3.4 MP12 | PB 9.0.3.2 | NX11.0.2.7 MP13 | PB 11.0.2 | VERICUT 7.3.4

Re: IPW turn first, mill and then finish turn

Master
Master

Doesn't my setup look like the one you screenshot? Am I missing something? Thanks 

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000

Re: IPW turn first, mill and then finish turn

Pioneer
Pioneer

Interesting! The NX understands this structure in Geometry? 

I normally do a separated Workpiece and MCS for milling operation. In my case the milling operations are simple, but the simulation isn't real.

Engineer and NC Programmer
NX 12.0.2 mp5

Re: IPW turn first, mill and then finish turn

Master
Master

I ended up just putting the mill mcs under main lathe mcs bypassing the ipw completely and it went back to the way it was with the correct ipw on the finish lathe ops. Not optimal but it worked this time for what I needed to do.

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000

Re: IPW turn first, mill and then finish turn

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The switching between machining modes has improved in NX 12 and later, but I think there is no way to directly support this scenario in NX 11 and below. For the older releases you need to cheat.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information