Cancel
Showing results for 
Search instead for 
Did you mean: 

IR 9350251: Add Tilt Tool axis inside dialogue for any operation it supports

Legend
Legend

Working on a big mirror image program (300 + operations ) (part is 100 lb block of titanium that goes down to 1.5 lbs) and just realized you cant mirror image any operations that have been tilted. Have to go back and recreate them. If tilt was built into the operation mirror image would be supported.

 

Hopefully more people here can add to my IR so we can see this added in the not so distant future.

 


Dennis Rathi
Creations Unlimited

Learn online





Solution Information