Cancel
Showing results for 
Search instead for 
Did you mean: 

ISSUE RELATED TO REST MILLING

Valued Contributor
Valued Contributor

HI

I am practicing on rest milling operation in NX cam.

I have machined two pockets with a End Mill of 30mm Dia with Cavity mill operation.

Now i want for the rest milling of these pockets with the end mill of 6mm of Dia but in rest milling , toolpath is not just limited in the corners rather it is spreads every where in pockets just like cavity mill operation.

I know a technique of Specifying trim boundaries to limitize the tool only to the corners but i want to know how to clean these residual corners without specifying trim boundaries.

my part model is attached here.Rest mill.JPG

9 REPLIES

Re: ISSUE RELATED TO REST MILLING

Valued Contributor
Valued Contributor

Aagha,

Try going into the cutting parameters

under the containment tab reference tool

call up your 30 mm cutter

re generate

try that

Re: ISSUE RELATED TO REST MILLING

Legend
Legend

Under mill_contour, the process called Zlevel Corner would do exactly what you are looking for...

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Re: ISSUE RELATED TO REST MILLING

Valued Contributor
Valued Contributor

Kinda of forgot

we go into verify and under the 3d dynamic tab hit the play button then create a ipw after it plays

use the ipw you created for the blank on the tool path that you want to use the 6mm cutter with

then we go into the cutting parameters and use the reference tool as described in last reply

Re: ISSUE RELATED TO REST MILLING

Valued Contributor
Valued Contributor

@robber80

 thank you for helping me in solving my problem.. 

Re: ISSUE RELATED TO REST MILLING

Siemens Phenom Siemens Phenom
Siemens Phenom

The settings in the Containment tab of the Cutting Parameters will help you with what you want. Rest Milling is initially set to use Level Based IPW, but changing this to 3D IPW gives you the additional option of specifying a Reference Tool. If you use the Reference Tool option and select that 30mm diameter tool you previously cut with, your cuts will now be limited to the inside corners where the reference tool could not reach.

Re: ISSUE RELATED TO REST MILLING

Valued Contributor
Valued Contributor

and what paul said

z-level corner works great on corners  (but not for floors)

 

Re: ISSUE RELATED TO REST MILLING

Valued Contributor
Valued Contributor

we find that the generation time is a lot longer when using 3d ipw

thats why we create an ipw through verify

Re: ISSUE RELATED TO REST MILLING

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I know this is solved but isn't the problem that the operations don't share the same workpiece parent?

Capture.PNG

LMGi
www.TLMGi.com

Re: ISSUE RELATED TO REST MILLING

Valued Contributor
Valued Contributor

In the "best practices" world you are absolutly correct

Learn online





Solution Information