Cancel
Showing results for 
Search instead for 
Did you mean: 

[ISV SETUP] Settings for MILLTURN MACHINE.

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi.

 

I refer to sim15_millturn_9ax in the library.

 

However, the axis direction is different from the equipment I want to set.

 

The Y-axis direction of the OOTB has an angle, and the equipment I set is at zero angle.

 

111.jpg

 

For example, moving the Y axis by 200 results in the following differences:

 

222.jpg

 

 

Where should I fix it?

 

 

3 REPLIES 3

Re: [ISV SETUP] Settings for MILLTURN MACHINE.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

the non orthogonal settings are within the MCF file 'sim15_millturn_9ax_fanuc.MCF'

 

The non orthogonal configuration is compensated with the TRANSY transformation.

2018-03-27 12_41_56-Machine Configurator - [E__NX_DEV_unit_feindNX1202_cam18004.2.2_FanucTNCCCFClean.png

 

This transformation is activated with initialization of cse (Pressing Simulate Machine) in method CSEInitializeChannel.

2018-03-27 12_41_04-XML Notepad - C__Users_feind_AppData_Local_Temp_re_md_tp_1522147208271.xml.png

 

Simply delete the entire Command node 'ActivateTransformation' and the 'TRANSY' transformation from transformation stack.

 

Thomas

Re: [ISV SETUP] Settings for MILLTURN MACHINE.

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

thank you thomas.

 

However, even after removing 'ActivateTransformation' and the 'TRANSY', it does not change.

222.jpg

 

Please confirm.

Re: [ISV SETUP] Settings for MILLTURN MACHINE.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello

M90 and TRAFOOF activate that transformation too inside the MCF.

Check if that is used or simple remove that too inside the meta codes.

 

Thomas

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information